FB#.SCALED.DIR

Description

FB#.SCALED.DIR sets the direction of the scaled feedback FB#.SCALED.P relative to the position feedback FB#.P.

Value Description
0 Non-reversing
1 Reversing

Versions

Action Version Notes
Implemented 02-07-02-000

General Information

Type

Read/Write

Units

N/A

Range

0,1

Default Value

0

Data Type

Integer

See Also

FB#.SCALED.P

Stored in Non-Volatile Memory Yes

Variants Supported

All variants are supported.

Related Topics

Scaled Feedback